Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
what is portable
Portable or flexible cable is used for temporary power. It is designed to be used in applications requiring less than 2000 volts. The cable has been designed to be flexible along with the ability to withstand harsh environments and varying temperature conditions. Portable cable can be manufactured using two basic materials: Thermoset Rubber or Thermoplastic PVC (Thermoplastic Elastomer).
PTM Veröffentlicht am: