Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
shielding
A shield is a metallic layer placed around a conductor or group of conductors. Shielding protects against electromagnetic interference (EMI), more commonly known as noise. Noise can be internal or external to the cable. Internal noise occurs when a varying magnetic field generated by one conductor induces a voltage on another conductor in the same cable. External noise is generated by EMI sources such as electric motors, fluorescent lighting, and variable frequency drives that come in contact with cables. Shielding utilizes a physical property of conductive enclosures which cancels externally generated EMI. The most common types of shielding are braided, spiral, foil, and a combination of foil and braid.
PTM Veröffentlicht am: