Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Slide26

A quick comparison between Renesas' ISL8088 and two competitive devices is shown on this slide. As seen from the table, the ISL8088 meets or beats the equivalent competitive ICs. The ISL8088 integrates two channels that switch in-phase similar to competitor 1. This reduces cross-mode jitter or channel interaction without having a significant impact on input filter requirements. The ISL8088 differentiates itself from the competition thanks to its feature set.

PTM Veröffentlicht am: