Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 10
Class D amplifiers, often incorrectly called digital amplifiers, are simply a continuation of the A, B, and C classification. A Class D is basically an audio modulated, PWM utilizing a saturated output stage such as those using power FETs. It is an amplifier where the output transistors are switched in the fully ON or OFF region. The outputs are continuously switched from one rail to the other at a high frequency. High efficiencies of up to 95% can be achieved, which leads to more compact products by eliminating the large heatsink which dissipates much of the usual heat. The one drawback of Class D amp is the high level of EMI emissions.
PTM Veröffentlicht am: