Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 4
NXP Class D audio amplifiers have a unique feature called Thermal Fold Back. If the junction temperature exceeds the threshold level (Tj > 140° C), the gain of the amplifier is decreased gradually to a level where the combination of dissipation and the thermal resistance from junction to ambient results in a junction temperature around the threshold level. This means the device will not completely switch off, but remains operational at lower output power levels. Especially with music output signals, this feature enables high peak out power while still operating without any external heat sink.
PTM Veröffentlicht am: