Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 5
NXP Class D audio amplifiers can distinguish between an impedance drop of a loudspeaker and that of a low-ohmic short-circuit across the load, or to one of the supply lines. In case of an impedance drop (for example due to the dynamic behavior of the loudspeaker) the maximum output current is limited to the allowable maximum current, but the amplifier will not switch off completely, thus preventing audio holes from occurring. The result will be a clipping output signal without any artifacts. This is called current limiting, and will result in NXP amplifiers becoming less sensitive to load and supply modulation.
PTM Veröffentlicht am: