Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Class D Audio Amplifiers Slide 27
This slide provides information on the Thermal Feedback feature of both the TDA8920C and TDA8920B. The TDA8920C can maintain the output power for a longer time when compared to the “B” version. The “B” version will shut down when over temperature protection goes into effect. Because of the higher supply voltage used with the TDA8920C, it produces less heat (requiring a smaller heat-sink); significantly improved THD; and less power loss in speaker wires due to lower speaker current.
PTM Veröffentlicht am: