Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Semiconductor General Purpose 24 Volt Motor Drivers Slide 15

The motion of the drums in slot machines is not random mechanical motion. Because they must be precisely controlled and brought to a sudden stop, a stepper motor is used. In the example of playing the crane game, it is obvious that it is not precisely controlled. In the game shown on this slide there are five brush motors in use, one for each axis of motion and two in the claw as shown in the drawing on the right.

PTM Veröffentlicht am: