Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Semiconductor General Purpose 24 Volt Motor Drivers Slide 6

In the block diagram of a cash machine, there are three separate units, the bill handling unit, coin handling unit, and the coin hopper. The bill and coin units have to align the currency for sensors to validate them as well as deliver them to the user. The coin hopper will return what has been input if the user pushes the return button. While some of these units are stand alone for making change, most of them are usually part of bigger machine like a snack or beverage dispenser. The standard power supply in these machines produces 24 volts and each of the units has multiple applications of 24 V motors.

PTM Veröffentlicht am: