Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Semiconductor General Purpose 24 Volt Motor Drivers Slide 24

The flow chart for industrial machines is similar to the cash machine. It should be remembered that stepper motors are for precise positioning control and if they have micro-stepping capability, they can also be used to reduce the vibration in the motors. Brushed DC motors and their drivers are typically less expensive than their stepper counterparts. Therefore if precise positioning is not critical, this type of motor is usually chosen. Some of these H-bridge drivers support more than one channel, be certain to verify how many channels are needed.

PTM Veröffentlicht am: