Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Semiconductor General Purpose 24 Volt Motor Drivers Slide 25

Shown on this slide is the H-bridge motor driver that was chosen to operate the claw in the crane game discussed previously. It used two motors so this dual channel part was a good match for the application. The FETS that drive the motors have a low ON resistance, therefore not much power is lost in the driver. This will operate from 9 to 35 V and can provide 2.5 A of output current. The LV8740V is available in a 44 pin SSOP package and there is an evaluation board available.

PTM Veröffentlicht am: