Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide13

One common question asked of Pulse Electronics, a YAGEO Company is; “why are there three pads on the board and only two on the antenna?” The short answer is that the feed point and backside short, required for function of a PIFA, is accomplished by the pad on the antenna shorting the two pads on the PCB. The board pads are normally kept separate to make impedance matching more stable and straight forward.

PTM Veröffentlicht am: