Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide7

As noted previously, the ideal helical monopole location is in the corner of the PCB. Note the corner mounting position on the PCB in the illustration on this slide in the radiation pattern of the XZ-PLANE. The object in the pattern is an image of a reference board with the surface mount antenna in the top left corner of the board. The E-Plane is in the same vertical plane as the length of the PCB; not broadside to the radiator. This illustrates the dependency of the ground plane as the ground plane and helical monopole both make up the aperture of the antenna. As the ground plane is reduced, the radiation efficiency also decreases. The helical monopole offers excellent omni-directional performance in the azimuth plane. Just as a dipole radiates omni directional with naturally occurring nulls in the zenith, so too is this evident in the helical monopole’s radiation pattern. Typical radiation efficiency for helical monopoles ranges between 50 to 55% peak efficiency.

PTM Veröffentlicht am: