Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide2

There are a some key points to consider when selecting the appropriate antenna for a device and/or application. The first question is; when in use, is the device handheld or must it work as a stand-alone unit? The next point should be where on the PC board the antenna should be located and if this is a fixed location. Another important consideration is whether there are any major components on the board or in the device, such as an LCD or a display, that may affect the antenna performance. The intended application, placement on board, board size, and circuit topology (to include the display) are all considerations that should direct the designer towards a specific antenna solution.

PTM Veröffentlicht am: