Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide5

The ideal location for the ceramic monopole antenna is in the corner or on the edge of the PCB.  The pattern in the top-left, marked XZ-PLANE, shows the image of the ceramic monopole across the top edge of the board. The E-Plane is in the same vertical plane as the length of the PCB, not broadside to the radiator. This is due to the coupling of the monopole to the ground plane. The ceramic monopole offers excellent omni-direction performance in the azimuth (XY) plane. Radiation efficiency is frequency dependent, but ranges between 50-70%.  The actual performance of the ceramic monopole is completely dependent on the mechanics. Displays, such as an LCD, or keypads can change the radiation characteristics of the antenna.

PTM Veröffentlicht am: