Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide11

Channel ID variables (marked with an * on this slide) can be re-configured at each message period, allowing  flexible  network performance and ad hoc reaction capability. Many ANT channel options open an RX window as part of the transmission phase providing ANT with an indication if there is any RF noise at that frequency and time slot that may prevent a good reception of the message. ANT will then delay the transmission ever so slightly to bypass the noise. Testing the new version of ANT has proven  that it can manage close to three hundred other ANT nodes occupying the same frequency and network within range of each other without collision damage. That performance was found to be necessary in fitness class applications with many ANT nodes in close proximity to each other.

PTM Veröffentlicht am: