Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide6

The serial message protocol that is the heart of ANT is well defined and currently is comprised of fifty messages that enable the developer to quickly define radio operation and data transfer in and out of the device. Since the protocol is embedded in the silicon there are no variables in interpretation of the network implementation such as take place in SDO based protocols and therefore no testing for adherence is needed, vastly reducing development, deployment and commercialization time and costs. Comparable design efforts to conceptualize and duplicate this backward compatible protocol would entail many years of work. Backward compatibility is one of the challenges developers face when making a family and generations of products for marketplace.

PTM Veröffentlicht am: