Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide9

An ANT channel is between the master and slave endpoint. The master endpoint is always transmitting (the primary transmitter). As mentioned earlier, ANT is mostly used as an isochronous network protocol. A decision to manage the trade off between data latency and battery life must be made. At this point the predominant variable in this decision is the number of messages sent from master to the slave per second. In ANT talk this is known as the channel period, which ANT allows to be configured very finely between 0.5-200Hz. Each message is comprised of a small overhead and eight bytes of user defined data. Messages are clocked over the air at 1MHz  and each message uses the radio for only 150µS.

PTM Veröffentlicht am: