Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide20

To make it feasible to service many more nodes than eight on a single channel, ANT has a channel option called shared. Just as the name indicates many receiver nodes share the same channel and are managed by the collection node that in this case acts as a master. The sharing takes place when the master sends a message during the regular message period and all slaves share in receiving the message. Within that message is a sixteen bit address that occupies the first two bytes of the standard eight byte ANT packet. Only the slave that is configured to the transmitted address responds. This address is known to the master and is used to individually select the slave the master wants to communicate with. The master will then move to another address based upon a polling order established by the application.

PTM Veröffentlicht am: