Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide34

As the simple PAN topologies ANT first created expanded, it was found to be necessary to connect to external data structures like PCs, fitness hardware, access points, etc. to deposit the collected data for review by the user/system. Therefore, it became necessary for ANT to make that connection easy for the ANT developer. Like most ANT developments, this solution was created first for ourselves and then supported once proven and robust in ANT-FS. ANT-FS (File Share) is a comprehensive state machine that allows a battery worn collection unit the ability to be discovered, authenticate its pedigree and contents and subsequently transfer them; all while the user is uninvolved with the process. Applications in the health space require a secondary level of security for personal data, so an AES128 engine and process were added to ANT-FS. ANT-FS uses a burst channel for data transfer so most files are transferred in less time than it takes to take the device off the body, allowing quick and reliable access to the data. This speed also supports a pass-by download, for example in corporate wellness data retrieval systems at work. To help consolidate, compress and extend the data files created by these collection units, the FIT file system was created. Both ANT-FS and FIT are supported by their own downloadable SDKs.

PTM Veröffentlicht am: