Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide23

Establishing the right data connection once RF connectivity is established is the next task. The application needs to make a decision as to what node it will connect with. Nodes may be built by the same vendor and sold as a package, they can be programmed to connect only with each other or they can take a truly ad hoc methodology to connecting. Identifying the master is the first step in that decision tree. Once the ID has been made the next decision is whether or not to pair.

PTM Veröffentlicht am: