Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
ANT-Slide21

Despite the fact that a synchronous network is the most power friendly option, there are some use cases that do not have the benefit of the time required to synchronize communications between nodes. ANT has an asynchronous channel option called the scanning mode. Basically the scanning mode is not a channel as the receiver configuration is on constantly. Continuous current consumption of 18mA demands a higher power source like a USB port or large battery capacity. No other receive or transmit functions are possible during the scanning mode as the complete radio is dedicated to this function. The back channel can be used to acknowledge and respond to the transmitters as they pass through the RF range of the scanning node.

PTM Veröffentlicht am: