Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
CRP

In order to protect application code and data, different levels of security can be enabled to restrict access to the on-chip Flash. There are three levels of code read protection (CRP) including CRP1, CRP2, AND CRP3. CRP1 disables access to the chip via the JTAG and allows a limited set of instructions in the systems programming (ISP) commands to update the Flash. This mode allows the Flash to be updated in the field but protects certain sectors from being overwritten. CRP2 also disables access to the chip via the JTAG and also limits the Flash updates to a global erase and update via ISP. CRP3 fully disables any access to the chip via the JTAG and the ISP so that the Flash is fully secured.

PTM Veröffentlicht am: