Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Clock Source

This illustration shows the clock tree on the LPC2300 and 2400 microcontrollers. As you can see, the ARM7 core can be clocked from the main oscillator, the IRC, or the RTC crystal. The WDT can be fed from the IRC or the RTC. Finally, the peripheral clock is divided down from the PLL clock, with each peripheral having its own divider as well for maximum flexibility.

PTM Veröffentlicht am: