Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Periph

Microcontrollers can often become slowed down while performing multiple simultaneous tasks due to bottlenecks on their internal bus structure. This is compounded by high quality graphics demanded by many current applications. Rather than the common solution of an MCU operating at several hundred MHz, NXP implemented a dual-AHB bus structure on the LPC2300 and LPC2400 series, which reduces the burden on the internal buses and allows concurrent operation of the zero wait-state Flash, 10/100 Ethernet, and LCD. These are the only low cost 32-bit MCUs that can achieve this level of performance.

PTM Veröffentlicht am: