Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
USB On-The Go
All LPC2400 series and some members of the LPC2300 series support USB Host and On The Go (OTG). The USB Host function allows the MCU to interface with USB devices attached to the bus. This function features two downstream ports, supports per-port power switching, and doesn’t require an external PHY. The USB OTG functionality integrates the host and device controller while the dedicated I2C interface controls any external OTG PHY compliance with the OTG transceiver specification. USB OTG supports any OTG transceiver that is compliant with the OTG transceiver specification in the USB 2.0 specification.
PTM Veröffentlicht am: