Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Powering FPGAs with SIMPLE SWITCHER LMZ3 Power Modules Slide 23

The WEBENCH Export option will take any WEBENCH power design that is enabled for export and convert it on-the-fly to leading CAD development platforms. Designers can export board layouts or schematics immediately from the custom designs created online in the no-cost WEBENCH Designer or Architect platforms directly into the customers CAD software, eliminating errors and saving design time. With WEBENCH Export, just open a design in this software just as if it took days or weeks creating it natively. WEBENCH Export allows the direct download of dynamic WEBENCH designs into leading CAD environments in minutes. Some of the key WEBENCH Export features include: Export makes designers more successful and faster to market than the competition. Create and optimize a custom power supply design using WEBENCH Designer. Run electrical and thermal simulations to characterize the design. Schematic Export gives the ability to download the schematic into popular CAD tools. Use PCB Export to export the PCB layout directly into the CAD tool. Export is supported by schematic and footprint layout symbols for 1,000 TI components, which join the 40,000 passive component library in WEBENCH tools supported by 115 ecosystem partners.

PTM Veröffentlicht am: