Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Powering FPGAs with SIMPLE SWITCHER LMZ3 Power Modules Slide 9

The output voltage also varies over load transient or fast changes in the load. This is analogous to the FPGA changing from a standby state to a high active state. In this case, the current is changed abruptly from 0 to 3 A and produces a 2% variation. Again, more output capacitance will help lower the voltage peaks and overshoots during a load transient since the peaks and overshoots are related to the capacitor equivalent series resistance. The next component to check is the output voltage ripple. As a DC/DC converter switches, the ripple will introduce a variation of the output voltage. The ripple is easily remedied by adding more output capacitance to lower the equivalent series resistance. In this case, the voltage ripple adds 0.05% to the voltage accuracy. Once again, voltage accuracy is dependent on several of the factors shown. The best way to approach voltage accuracy is to find a device with a good performance in each category.

PTM Veröffentlicht am: