Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
device enum1
USB devices report their attributes to the Host using descriptors. A descriptor is a data structure with a defined format. The Device descriptors represent the entire device, hence there is only one device descriptor per device. It specifies USB version, maximum packet size, Vendor, Product IDs, and the number of possible configurations. The Configuration descriptor provides what a USB device needs to have configured before its function may be used. The Host is responsible for configuring a USB device. Within a single configuration, a device may support multiple interfaces.
PTM Veröffentlicht am: