Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
usb data flow2
The USB device layer is typically responsible for providing the data in a specific format used by the functional layer. If the device operates through a HUB, then the logical layer is responsible for carrying out the respective data rate translations. Data from Win32 COM APIs originating from a PC flows to the USB BUS drivers which actually controls the hardware to transmit USB packets. The Bus drivers are responsible for routing the data and polling the status of the device operation. The Bus layer also provides over-current protection and power management.
PTM Veröffentlicht am: