Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
vinc1
There are several pre-compiled firmware options available to carry out different tasks using the VNC1L. VDAP (Vinculum Disk And Peripherals) provides the monitor port on the combined interface. USB Port 1 is configured for Host operation and supports HID, Printer, Hub, CDC, and FTDI peripherals. USB Port 2 supports these same devices and adds support for BOMS. VDIF (Vinculum Disk and FTDI monitor) is similar to VDAP except when an FTDI peripheral device is detected on PORT1, the monitor port is disabled on the combined interface and shifted to USB Port 1. VDIF only supports BOMS, HID, and printer devices on Port2.
PTM Veröffentlicht am: