Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
ftdi device6
Extended APIs provide access to additional features, such as programmable receive buffer timeout and bit bang modes. FT-Win32 APIs are a more sophisticated alternative to the Classic Windows COM API. They are equivalents to the native Win 32 API calls that are used to control a legacy serial port. Using the FT-Win32 API, existing Windows legacy communication applications can easily be migrated to use the D2XX interface simply by replacing the standard Win32 API calls with the equivalent FT-Win32 API calls.
PTM Veröffentlicht am: