Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
usb data flow1
There are three layers of operation happening when a device is interacting with a host controller: the functional layer, USB device layer, and the USB bus layer. On the Host side, the functional layer of PC applications sends data to or from the device. For example, an RS232 terminal application, like HyperTerminal, forms the USB functional layer which displays the data received or transmits data to the USB device. The HyperTerminal application may use standard Win32 COM APIs which, in conjunction with a USB device driver, will logically convert that data back and forth from USB packets.
PTM Veröffentlicht am: