Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
tools3
For Host Specific Tools, VNC_PROG programs firmware into a VNC1L using the VPROG1 programmer. Up to 10 VPROG1 units may be used at a single time. VPROG1 is a single unit Vinculum programmer with optional adapters to program unmounted ICs in a PLCC ZIF socket or VDIP modules through a DIP ZIF socket. V-Eval is a VNC1L development board with an application utility to quickly prototype designs using the VNC1L. The V-Eval provides a VNC1L monitor port interface to a host PC through the use of an FT2232D device. The same interface is also used to program firmware and observe the UART monitor port of the VNC1L when used with external circuitry. The V-Eval also provides ample PCB area for implementing prototype designs.
PTM Veröffentlicht am: