Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 11

This shows a competitive typical Full Duplex RFID system. Because the reader is always transmitting, the associated noise can be a problem. Full Duplex means that signals travel in both directions at the same time. The reader block diagram shows that the primary winding is part of the reader's resonant antenna circuit while the secondary winding is part of the transponder's resonant circuit. Also, shown are the transmission signal waveforms for the reader and transponder. To communicate, the reader creates a powerful carrier signal which causes the transponder’s resonant circuit to oscillate. These oscillations create an oscillating magnetic field which is amplitude modulated by the transponders control circuitry and used to send data back to the reader.

PTM Veröffentlicht am: