Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 6

It was mentioned earlier that communication between the tags and the reader is by radio waves. These waves have a magnetic and an electric component. Both LF and HF systems use the Magnetic or "H" field to transfer energy to a tag by induction. This creates a homogeneous RF field but the strength of this field falls off sharply. UHF systems use the Electric field to transfer energy to a tag by propagation. The strength of this field doesn't fall off as quickly as the magnetic field, giving UHF tags an extended reading range but reflected signals result in a reading zone that is less well defined.

PTM Veröffentlicht am: