Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 13

Texas Instruments' Half Duplex system looks very similar to the Full Duplex system. However, there is an additional charge capacitor in the transponder. When instructed, the reader activates its transmitter for 50 ms, which is long enough to charge the capacitor. The transmitter is then turned off and the transponder responds using the energy stored in the capacitor. Half Duplex means that signals are only traveling in one direction at a time. More importantly, the tag does not have to compete with any noise associated with the powerful carrier signal. The response signal is frequency modulated which allows superior performance in noisy conditions and a better ability to discriminate between closely spaced tags.

PTM Veröffentlicht am: