Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 5

There are only certain frequencies in the radio spectrum where tags are allowed to operate and depending on the frequency, tags can have different operating characteristics. This slide shows part of the radio frequency spectrum, unfortunately most of this finite resource was allocated long before RFID. So RFID is now limited to three main bands; Low Frequency (LF) band between 120 and 134 kHz, High Frequency (HF) band at 13.56 MHz and Ultra High Frequency (UHF) band between 850 and 960 MHz. Associated with each band are International standards which will be reviewed later.

PTM Veröffentlicht am: