Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 19

Another advantage of LF RFID is its well defined read zone which is evident in automotive immobilizer systems. The reading distance from the key to the steering column lock needs to be well defined to avoid reading any other keys on the ring. This technology was first adopted in 1993 and since then it has been adopted by almost all automobile manufacturers. Another application that takes advantage of the well defined reading zone are pay the pump systems which use a keyfob as a credit card. The LF system’s well defined reading zone allows the reader to charge the correct tag without affecting a customer's tag on the other side of the pump.

PTM Veröffentlicht am: