Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 2

Radio Frequency Identification is a technique that uses short range radio transmissions for collecting information on people, animals, and products. This information may include identity, position, time, or financial transactions. Unlike barcodes which only identify product groups, RFID tags can have a unique number for each product. Identification is performed in milliseconds and line-of-sight is not required. There is no contact between the tag and reader which allows multiple tags to be read simultaneously. The tags can also work in harsh environments or be implanted under the skin for pet identification and livestock tracking.

PTM Veröffentlicht am: