Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 31

UHF RFID systems are required to work at different frequencies depending on the country of operation. For example, in the USA they can operate between 908 MHz and 928 MHz, while in Europe they operate from 865 MHz to 868 MHz. Not only does the frequency vary with country of operation but so does the RF power that can be legally transmitted. It is 4 Watts Effective Isotropic Radiated Power (EIRP) in the USA but only 2 Watts Effective Radiated Power (ERP) in Europe.

PTM Veröffentlicht am: