Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 22

HF tags operate at 13.56 MHz giving a wavelength of approximately 22 meters which is much shorter than the 2200 meters of low frequency RFID systems. This frequency is available worldwide at adequate power levels, without special licensing. The radio waves will still pass through materials with the exception of metals. However, unlike LF systems, some energy is lost which results in reduced range. HF Tags mainly use a flat label format with etched flexible antennas. The magnetic field is still used to power the tag, so HF systems also have a well defined read zone. HF systems are also capable of reading multiple tags in a RF field simultaneously (up to 60 tags a second).

PTM Veröffentlicht am: