Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
vf temp
The characteristic behavior chart for the input Forward Voltage vs. Ambient Temperature for a Solid State Relay is shown here. As can be seen, for the input Infrared Emitting Diode (IRED) the Forward Voltage decreases with increasing temperature. Therefore, the input circuit design should consider this change in Forward Voltage over temperature in order to select an appropriate resistor value for the input. Even though the amount of change is small as compared to other system voltages, the designer should ensure that the change in Forward Voltage does not place the input drive circuit at the limit of the design. Also, the Forward Current may drop slightly due to driver resistance changes in the circuit.
PTM Veröffentlicht am: