Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
factors affect off
The SSR will actually turn off faster when the input IRED has been driven harder. As shown in the graph for Normalized Turn-Off Time vs. Temperature, the characteristic of this SSR will turn off slower when above 25°C. This is dependent on the specific SSR type. Again, the designer needs to take into account the operating temperature environment and make allowance for all component tolerances over the full range of expected temperature, voltage, and current conditions.
PTM Veröffentlicht am: