Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
ssr type
A normally-off type SSR (which is functionally the same as a “make contact” mechanical relay) leaves the output terminals open if there is no input signal, and short-circuits the output terminals if an input signal above threshold level is applied. Conversely, a normally closed type SSR (which is functionally the same as a “break contact” mechanical relay) keeps the output terminals short-circuited if there is no input signal, and opens the output terminals upon correct application of an input signal.
PTM Veröffentlicht am: