Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
turn on
Note that the turn on time for the SSR is greatly reduced with input Forward Current above a few milliamperes and below 0.4 msec for a forward current greater than 5 mA. The recommended operating conditions shown in the table below indicate the Typical Forward Current of 10 mA should provide a turn-on time of 0.2 msec. A minimum Forward Current of 2 mA will cause the device to operate, however the turn-on time will be 1 msec or longer, as seen in the graph, Turn-On Time vs. Forward Current for the PS7241-2A. Also, the graph gives some idea about the likelihood of any individual SSR behaving within the scope of the parameters in the data sheet.
PTM Veröffentlicht am: