Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
pe diss
This slide details the calculation of the input power dissipation of the IRED in the SSR. The data used in these calculations was obtained from the graphs depicted on the previous slides associated with the PS7241-2A device. As shown here, the input power consumption is calculated to be 12 mW.
PTM Veröffentlicht am: