Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
on res
The channel resistance characteristic trends towards higher resistance with higher temperature. In the graph shown here, the load current is 120 mA on the output of the SSR. The distribution graph shows that 17 pieces of this SSR have an On channel resistance of 24 Ohms, 27 pieces have a resistance of 25 Ohms, and 6 have a resistance of 26 Ohms. Therefore, the “on” resistance of these devices is very consistent in each batch of these products.
PTM Veröffentlicht am: