Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
basic int comp
Compared with a mechanical relay, the input and output control sections, made up of the IRED and PVD in the OC MOSFET, correspond to the function of the coil in the mechanical relay. They isolate the input from the output and generate the open or closed action on receipt of an input signal. Unlike a mechanical relay, an input coil catch diode is not required, as the inductor kick of the mechanical relay coil is not present. The output MOSFET in the SSR corresponds to the contact in the mechanical relay, opening and closing the load circuit.
PTM Veröffentlicht am: