Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
po diss
The output-side power dissipation is calculated as follows: PO = Iload2 x R(on) x duty cycle where Iload is the maximum DC output current. Using the previous graphs for the PS7241-2A, the main portion of the distribution is at 25 Ohms and this will be used for the example. The Duty Cycle will be considered “1” for this case where the SSR is considered “On” and power calculations for high-rate switching conditions will not be considered here. From the calculations shown here, the output power is 360 mW.
PTM Veröffentlicht am: